Safety Precautions
If the equipment is used in a manner not specified by the manufacturer, the protection provided by the equipment may be impaired.
Before Starting Work
Before starting work, qualified personnel and the operator must have read and understood this document. Follow all instructions.
Modifications and repairs to the product may only be carried out by Schneider Electric employees, if expressly permitted by the instructions of this document.
Instructions and symbols directly attached to the product must be observed. They must not be removed and must be kept in a fully legible condition.
People Authorized to Install the ProbeSensor
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Safety Checklist
-
Is the transformer de-energized and lines grounded (LockOut TagOut procedure followed)?
-
Is the transformer temperature less than 40 °C (104 °F)? Record the temperature by reading the transformer oil temperature indicator or by using a laser thermometer.
-
The EcoStruxure™ Transformer Expert ProbeEcoStruxure™ Transformer Expert Sensor H2 (hereafter referred to as ETE ProbeETE Sensor) may be installed on the top oil valve or the External Temperature Sensor installed around the top pipe to the radiator. Are these parts safely accessible from ground-level?
-
Is appropriate personal protective equipment (PPE) available and used?
Transformer Operator’s Responsibility
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
CAUTION |
|---|
|
HAZARD OF hot surface
Failure to follow these instructions can result in injury or equipment damage.
|
-
Select appropriate probesensor to help ensure the proper functioning of the system or machine. Schneider Electric can only make recommendations based on our experience with similar applications.
-
Follow all safety instructions in this manual and additionally apply all local regulations.
-
Advise the installation team of installation risks and provide suitable control measures to help ensure the safety of staff.
-
Identify hazardous processes in the vicinity of the workplace and provide suitable control measures to help ensure the protection of installation staff.
-
Provide site-specific training before commencement of work, including site access and egress.
-
Provide emergency procedures and associated emergency telephone numbers (if applicable).
-
Check the legibility of the type plate.
Cleaning Instructions
The ETE ProbeETE Sensor is IP65-rated and requires cleaning once a year. Cleaning frequency increases in harsh environmental conditions (extreme cold or heat). During scheduled transformer maintenance, the probesensor may be cleaned to remove any accumulation of dust, oil, snow, or any other pollutants.
| NOTICE |
|---|
|
hazard of UNINTENDED equipment OPERATION
Do not use a high pressure water jet or any kind of chemicals
during cleaning.
Failure to follow these instructions can result in equipment damage.
|
End-of-Life Disposal of Equipment
This kit (including all accessories) is not intended for household use. At the end of its service life, do not dispose of the kit with household waste.
For customers in EU countries (including the European Economic Area), Schneider Electric is subject to the EU Waste Electrical and Electronic Equipment Directive 2012/19/EU (WEEE directive). As part of our legal obligations under this legislation, contact a Schneider Electric representative to recover the kit and make sure that it is disposed of by authorized recycling agents.
For customers outside the European Economic Area, contact a Schneider Electric representative to recover the kit and make sure that it is disposed of by authorized recycling agents in accordance with the local legal requirements.
For information:
-
The body of the ETE ProbeETE Sensor is made of aluminum, and the probefront cap is made of stainless steel. The body and probefront cap can be recycled.
-
Electronics (PCBA) are located inside the body of the sensor, which can be recycled according to local electronics rules.
-
The black end cap is made of plastic (acetal 7) and can be recycled accordingly.
Improper Use
| NOTICE |
|---|
|
Hazard of unintended equipment operation
Failure to follow these instructions can result in equipment damage.
|
The following chapters provide information on the installation requirements of the ETE ProbeETE Sensor kit.
DANGER
CAUTION