990-91386-001

Additional Safety Precautions After Installation

DANGER
hazard of electric shock, explosion, or arc flash
Do not install the UPS system until all construction work has been completed and the installation room has been cleaned. If additional construction work is needed in the installation room after this product has been installed, turn off the product and cover the product with the protective packaging bag the product was delivered in.
Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.