990-91459A-001

Specifications

Trip Settings

  Galaxy VL internal backfeed kit for UL (GVLOPT003) Galaxy VL internal backfeed kit for IEC (GVLOPT004)
Breaker type PLF34080CU33AAC NS1000H (33473)
Ir 1 0.95
tr ≥4 ≥4
li (x In) ≤10 ≤10

Torque Specifications

Bolt size Torque
M6 5 Nm (3.69 lb-ft / 44.3 lb-in)
M8 17.5 Nm (12.91 lb-ft / 154.9 lb-in)
M10 30 Nm (22 lb-ft / 194.7 lb-in)
M12 50 Nm (36.87 lb-ft / 442.5 lb-in)
QR code for this page

Was this helpful?