990-94383A-001

Remove the UPS from the Pallet

  1. Move the UPS cabinet as close as possible to the final location with a pallet truck or a forklift before unpacking.
  2. Remove the packaging (cardboard, plastic, and foam corners). Save the packaging bag (marked (A) in the illustration).
  3. Remove the ramp.
  4. Open the front door.
  5. Remove the front transportation bracket.
    NOTE: Save the front transportation bracket. It will be reused for seismic anchoring, refer to the UPS installation manual for details.
  6. Close and lock the front door.
  7. Attach the ramp to the pallet and remove the rear transportation bracket.
    NOTE: Save the rear transportation bracket. It will be reused for seismic anchoring, refer to the UPS installation manual for details.
  8. Roll the UPS carefully down the ramp.
    CAUTION
    Hazard of personal injury
    • Make a clear path in front of the ramp.
    • Do not stand in front of the ramp while rolling the UPS down the ramp.
    Failure to follow these instructions can result in injury or equipment damage.
  9. Move the UPS to the final location by rolling it over the floor on the casters.
    WARNING
    TIPPING hazard
    • The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
    • The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
    • Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  10. Cover the UPS with the packaging bag (marked (A) in the illustration) until time of installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?