990-5454C-001

Prepare the Empty Battery Cabinet for Cables – Bottom Cable Entry

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the cabinet.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the gland plates for (a) power cables and (b) signal cables.

    Front View of the Empty Battery Cabinet

  2. Drill or punch holes for power cables and signal cables in the gland plates.
  3. Reinstall the gland plates.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?