990-6363-001

Install the IP52 Kit on the UPS

NOTE: The IP52 kit can only be installed on a UPS with bottom cable entry.
NOTE: This procedure describes installing the IP52 kit after power cabling and signal cabling is completed. Rear access is required to install the IP52 kit on the UPS.
  1. Follow the UPS installation manual to install the UPS.
  2. Remove the front panel, the lower front plate, the transparent cover, the top cover, the left side panel (if present), and the right side panel.
  3. Mount the provided flat gaskets on the side panel(s) as close to the bottom and top inside edges as possible for optimal sealing.

    Inside View of the Bottom Part of the Side Panel

    Inside View of the Top Part of the Side Panel

  4. Reinstall the side panel(s) on the UPS.
  5. Remove the two brackets and the rear cover. Save the two brackets and the flat head screws and discard the rear cover.

    Rear View

  6. From inside the UPS, remove the rear gland plate.
  7. Mount the flat gasket 12.7 mm from the edges on the rear gland plate for optimal sealing and save the rear gland plate for later installation.
  8. From inside the UPS, install the two shown parts with the six provided M6 screws.
  9. From inside the UPS, install the two shown parts on the bottom gland plate with the existing screws.
  10. Disconnect the signal cables from the top of the UPS and pull the signal cables out through the rear gland plates on the UPS. Note the signal cable connections.
  11. Remove the gland plates (A) and the brush plates (B) from the rear of the UPS.

    Rear View

  12. Reinstall the two brush plates reusing the four screws. Save the gland plates for later installation.
  13. Reinstall the two brackets from step 5 and the shown part. Reuse the flat head screws from step 5.

    Rear View

  14. Install the two provided studs.
  15. Assemble the rear assembly:
    1. Install the rear gland plate from step 6 on the shown part reusing the M6 screws.
    2. Install the shown part with the two provided M6 flat head screws and nylon washers.
    3. Install the gland plates from step 11 as shown with the four provided M4 screws.

    Rear Assembly

  16. Reconnect all the signal cables in the UPS:
    1. Place the rear assembly up against the UPS.
    2. Route the signal cables through the signal gland plates. See routing instructions in the UPS installation manual.
    3. Reconnect the signal cables in the UPS. See connection instructions in the UPS installation manual.

    Rear View

    CAUTION
    Equipment damage
    Ensure that the signal cables are not damaged during this procedure.
    Failure to follow these instructions can result in injury or equipment damage.
  17. Reinstall the top cover:
    1. Tilt the top cover and slide it onto the UPS from the rear. Tabs in the rear of the top cover must connect to the slots in the rear of the UPS.
    2. Push the top cover down in the front.

      Rear View

      CAUTION
      Equipment damage
      Ensure that the signal cables are not damaged during this procedure.
      Failure to follow these instructions can result in injury or equipment damage.
  18. Install the rear assembly with the eight provided M6 flat head screws and nylon washers.

    Rear View

    CAUTION
    Equipment damage
    Ensure that the signal cables are not damaged during this procedure.
    Failure to follow these instructions can result in injury or equipment damage.
  19. Install the shown part reusing the M6 flat head screws from the top cover.
  20. Install the shown part with the four provided M6 flat head screws and nylon washers.
  21. Reinstall the transparent cover and the lower front plate.
  22. Remove the air filter from the front panel. Discard the air filter.
  23. Remove the display plate and the three gaskets from the front panel.

    Outside View of the Front Panel

  24. Mount the provided profile gaskets as shown and reinstall the display plate on the front cover.

    Outside View of the Front Panel

  25. Remove the top gasket from the front panel.

    Inside View of the Front Panel

  26. Mount the provided profile gasket as shown on the front panel as close to the edges of the front panel frame as possible. Start from the bottom centre and mount the profile gasket in one piece for optimal sealing.

    Inside View of the Front Panel

  27. Install the transparent plastic part in the bottom of the front panel.

    Inside View of the Front Panel

  28. Install the four provided cage nuts.

    Inside View of the Front Panel

  29. Install the shown part with the four provided M6 screws.

    Inside View of the Front Panel

  30. Attach the supplied label 885-92048 from the kit on the UPS lower front plate to alert to the risk of overheating.
  31. Reinstall the front panel on the UPS:
    1. Insert the two tabs in the bottom of the front panel in the UPS at a tilted angle.
    2. Reconnect the front panel strap to the UPS.
    3. Close the front panel and lock with the two locking knobs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?