990-91141L-001

Torque Specifications

Bolt size Torque
M4 1.7 Nm
M5 2.2 Nm
M6 5 Nm
M8 17.5 Nm
M10 30 Nm
M12 50 Nm
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.