990-91141K-012

Caractéristiques du couple de serrage

Taille de vis Couple
M4 1,7 Nm
M5 2,2 Nm
M6 5 Nm
M8 17,5 Nm
M10 30 Nm
M12 50 Nm
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?