990-91141L-006

Corriente residual

Instalación de sistema SAI 380/400/415 V de 4 conductores a plena carga

Potencia nominal del SAI Corriente residual
20-50 kW 62 mA
60-100 kW 67 mA
120-150 kW 91 mA
Comentarios
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.