990-91378D-001

Mount the Battery Breaker Kit in a Grounded Metal Box

CAUTION
risk of equipment damage
Mount the battery breaker in a grounded metal box.
Failure to follow these instructions can result in injury or equipment damage.
  1. Measure and mark the holes for mounting the battery breaker kit in the metal box.
  2. Drill holes in each of the marked locations.
  3. Mount the battery breaker kit in the metal box.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.