Unpack the UPS and the Modular Battery Cabinet GVSMODBC9
NOTICE |
---|
RISK of equipment damage
Do not unpack the cabinet before the time of installation.
Failure to follow these instructions can result in equipment damage.
|
NOTICE |
---|
RISK of equipment damage
Failure to follow these instructions can result in equipment damage.
|
- Remove all the packaging, retrieve the installation kits, and save the protective packaging bag for later use.
- Only for the UPS: Disconnect the two signal cables on the UPS.
- Remove the front door.
- Remove the M8x30 bolts and transportation brackets from the front of the cabinet. Save for later use.
- Remove the floor protection plate and the jack.
- Remove the bolts.
- Remove the side pallet parts.
- Place the floor protection plate under the pallet on the rear side of the cabinet. Place the jack into the transportation bracket hole and use a drilling machine to lift the cabinet up to the max height of the jack.
- Remove the rear pallet part.
- Use the drilling machine on the jack to lower the cabinet down to the floor.
- Move the transportation bracket, the jack, and the floor protection plate and install on the front of the cabinet.
- Lift and remove the front pallet part in the same way as the rear pallet part was removed. Remove the transportation bracket, the jack, and the floor protection plate.
- Only for the UPS: Reinstall six M8x30 bolts on the front and the rear of the UPS.
- Only for the modular battery cabinet: Reinstall the two transportation brackets with M8x30 bolts on the rear of the modular battery cabinet. Reinstall M8x30 bolts in all the empty holes on the rear and front of the modular battery cabinet.
- Reinstall the front door.
- Only for the UPS: Reconnect the two signal cables. Fasten the signal cables with cable ties in the upper left corner.