Remove the Power Cabinets from the Pallet (Type 1)
| NOTICE |
|---|
|
RISK of equipment damage
Ensure that the floor is level and can support the weight
of the jack when it carries the cabinet.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
RISK of equipment damage
Be careful not to damage the cabinets when using the jack.
Failure to follow these instructions can result in equipment damage.
|
- Use the installation kit 0M-816661 shipped with the I/O cabinet. Use the jack and the floor protection plate in the kit for all cabinets in this procedure.
- Place the floor protection plate under the pallet on the rear of the cabinet.
- Place the jack from the installation kit in the hole in
the transportation bracket on the rear of the cabinet.
WARNINGhazard of TiltingDo not use a jack in the front and rear transportation bracket at the same time.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Remove the bolts from the rear transportation bracket and from the middle pallet part. Remove the pallet parts marked with an (A) in the illustration and save for step 8.
- Use the electric torque wrench with the provided hexagonal
socket to operate the jack. Position the jack in the bracket, and
raise the jack until it has contact with the floor protection plate.NOTE: Reduce the drill torque to minimum to prevent kickback.
- Use the jack to lift the cabinet to the top position.
- Remove the rear and middle pallet parts and save the part marked with an (A) in the illustration for step 8.
- Place the pallet parts marked with an (A) in the illustration under the transportation bracket as support. The pallet parts are reused from step 4 and 7.
- Use the jack to lower the cabinet down onto the support.
- Move the floor protection plate and the jack to the transportation bracket on the front of the cabinet.
- Remove the bolts from the front transportation bracket.
- Use the jack to lift the cabinet to the top position.
- Remove the front pallet parts.
- Use the jack to lower the cabinet onto the floor until the casters connect with the floor. Remove the jack and the floor protection plate.
- Move the cabinet so you can remove the remaining pallet parts.
- Remove the front and rear transportation brackets from
the cabinet.
The cabinet can now be moved on the built-in casters to the installation area.
NOTE: Save the transportation brackets and bolts for later reuse. The transportation bracket is reused as front anchoring bracket.
WARNINGTIPPING hazard- The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention to the floor conditions and the balance of the UPS.
Failure to follow these instructions can result in death, serious injury, or equipment damage.