990-5453C-001

Unpack the Cabinets

  1. Cut the plastic wrap along the edges and remove.
  2. Remove the cardboard cover.
  3. Remove the corner protection.
  4. Remove the bag.
  5. Remove the kit parts from the pallet and the packaging and save for the installation.
    NOTE: Installation kits are also placed inside the I/O cabinet. Remove these when the I/O cabinet has been removed from the pallet.
  6. Cut the tape at the bottom of the cabinet and fold out the plastic bottom protection.
  7. Take the keys that are attached to the bags and save for later use.
  8. Remove and dispose of the silica bags.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?