Electrical Safety
This manual contains important safety instructions that should be followed during the installation and maintenance of the UPS system.
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
The label below must be added if:
-
The UPS input is connected through external isolators that, when opened, isolate the neutral, OR
-
The UPS input is connected via an IT power system.
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Risk of voltage backfeed. Before working on this circuit: Isolate the UPS and check
for hazardous voltage between all terminals including the protective earth.
Failure to follow these instructions will result in death or serious injury.
|