7EN02-0420-03

Configuring input output parameters

  1. Navigate to Menu > Settings > I/O Config.

    The I/O CONFIG screen displays.

  2. Modify the parameters value as per the following table:
    NOTE: Use the contextual menu buttons to modify the parameters value.
    Parameter Allowed Values Default Value Description
    Ins. Al. Relay
    • Std. (Standard)

    • FS (Failsafe)

    FS (Failsafe) Select the mode of insulation alarm relay depending on the status of insulation. Refer user manual for more information.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?