7EN72-0203-02

Remote display firmware version 4.0.10

PM89RD96 remote displays that have firmware version 3.x.x or earlier are not compatible with meters with firmware version 2.1.0 or later.

To use the PM89RD96 remote display with the meter, you must first upgrade the PM89RD96 firmware to version 4.0.10 (rmdupg_rd96_004.000.010).

For a detailed procedure on upgrading the PM89RD96 remote display firmware, download the PM89RD96 Display firmware upgrade technical note at www.schneider-electric.com/en/download/document/7EN72-0202

QR code for this page

Was this helpful?