43006–850–01

Section 1—Introduction

This instruction bulletin provides installation, operation and maintenance instructions for dry-type transformers 1000 volts and below for use in commercial and industrial applications.

NOTE: This bulletin should be used only by qualified personnel.

The following dry-type transformer product families are included in this instruction bulletin. Typical transformers are shown in Energy Efficient 2016
Transformers (EX)
, Energy Efficient 2016
Transformers (EX)
, Open Core and Coil, Energy Efficient (EE) Ventilated Transformer, Non-Linear (NL, NP, NLP) and
Harmonic Mitigating (HM)
, and Non-ventilated
Transformer
.

  • Low Voltage Distribution Transformers, Three-phase and Single-phase

    • General Purpose—50 and 60 Hz

    • Energy Efficient (EE)—60 Hz

    • Energy Efficient 2016 (EX)—60 Hz

    • Non-linear Offering (NL, NP or NLP)—50 and 60 Hz

    • Harmonic Mitigating Transformers (HM)—50 and 60 Hz

    • Open Core and Coil (OC)

  • Drive Isolation Transformers (DIT)

  • Non-ventilated Transformers (NV)

Energy Efficient 2016
Transformers (EX)

Energy Efficient 2016
Transformers (EX)

Open Core and Coil

Energy Efficient (EE) Ventilated Transformer

Non-Linear (NL, NP, NLP) and
Harmonic Mitigating (HM)

Non-ventilated
Transformer

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?