BQT8706400-03

Spacing Around the Switchboard

CAUTION
hazard of incorrect dimensions
Adhere to the specified spacing dimensions around the switchboard, refer to Figure 5.
Failure to follow these instructions can result in injury or equipment damage.

Figure 7
Top View of the Switchboard and Surrounding Spacing

The L dimension depends on the cubicles of the switchboard.

A: This dimension should be equal to:

  • 200 mm for AFL (Accessibility Front Lateral) type of cubicle.

  • Minimum 800 mm for AFLR (Accessibility Front Lateral Rear) type of cubicle.

B: 35 mm end cover.

C: Should be 800 mm for lateral access & 500 mm if no access.

D: Minimum 1200 mm for opening the door.

E: The dimensions are as follows:

  • Minimum distance for operating must be 1500 mm (minimum distance for face-to-face switchboard configuration must be 2500 mm).

  • 1550 mm for operation (extraction and positioning of mobile parts).

  • 2060 mm for the extraction of one cubicle with a depth of 1860 mm without displacing the others.

  • 1640 mm for the extraction of cubicle with a depth of 1440 mm and 1840 mm for the extraction of cubicle with a depth of 1640 mm without displacing the others.

  • To place the ramp and remove the Withdrawable VT (WVT) from the front side, a minimum of 2000 mm of space is required.

F: Main earth bar for the switchboard.

NOTE:
  • The cubicle is used for different cubicle setups, including feeder/incomer, bus coupler, bus riser, and bus metering configurations.

  • For the extraction of the cubicle, contact Schneider Electric field service.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?