BQT8706400-03

Assembly

Safety Provisions

WARNING
HAZARD OF TOPPLING
When handling the moving devices, pay attention to uneven floor surfaces (for example, cracks, projections and so on) of the switchgear room.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
HAZARD OF FALLING
  • Do not walk upon the topsides of the switchgear cubicles.
  • During civil engineering activities, when working on the top of the switchgear cubicles (such as during the installation of deflectors, fans, or pressure relief ducts), temporarily attach a sturdy base plate that is walkable.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Instructions for Assembly

MCSeT cubicles are delivered with E/S in ON position.

The VCBs are always shipped in open state (OFF) with the energy-storing device released.

NOTICE
HAZARD OF inappropriate assembly
  • Ensure there is no condensation, dirt, and dust during assembly of cubicles on all accounts.
  • Observe and read assembly drawings before commencing the assembly work.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?