Library File novA Products

Micrologic X (PSE1061)

For information about recommended action on events, refer to the relevant document:

  • MasterPacT MTZ1 - Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Units - User Guide

  • MasterPacT MTZ2/MTZ3 - Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Units - User Guide

VL “X_protective_cover” used in PSE1416 (repair procedures)

VL “X_EarthLeakageProtectionLoss” used in PSE1061(Micrologic X).

VL “24Vdc_SELV_use” used in PSE1061(Micrologic X).

VL “24Vdc_SELV_connection” used in PSE786 (ULP), PSE1061 (Micrologic X) incl. customized consequence (‘will result in a basic/single insulated system’).

Maintenance Procedures (PSE1217+1287+1416) and Maintenance Guide (PSE992)

VL “MaintenanceReco” used in PSE992+1217+1287+1416

VL “MaintenanceReco” used in PSE992+1217+1287+1416+ Compact NSX Twin PSE1539

Maintenance recommendations for each device are intended to maintain the equipment or subassemblies in a satisfactory operational state for their useful service life.

VL “MaintenanceOp” used in PSE992+1217+1287+1416+ Compact NSX Twin PSE1539

The following table summarizes maintenance operations for the three preventive maintenance programs:

Maintenance program

Maintenance description

Performed by

Routine end-user maintenance

Visual inspection and functional testing, replacement of inoperative accessories.

  • Trained and qualified end-user personnel

  • Trained and qualified maintenance services provider personnel

  • Schneider Electric Services representatives

Intermediate end-user maintenance

Routine end-user maintenance, plus operational servicing and subassembly tests.

  • Trained and qualified maintenance services provider personnel

  • Schneider Electric Services representatives

Manufacturer maintenance

Intermediate end-user maintenance, plus diagnostics and part replacements by Schneider Electric Services.

Schneider Electric Services representatives

VL “MTZ_VPS” used in PSE1079 MTZ2/3

VL “MTZ_VPS” used in PSE1287 maintenance

VL "MTZ_safety_FixedCB" used in D-SE-0057794 (Breaking Unit NIII_Z_1: Check the Condition of the Breaking Unit)

VL "MTZ_safety_FixedCB" used in D-SE-0057803 (Chassis NIII_Z_1: Dust and Grease Chassis)

VL “GeneralSafety_RiskEquipmentDamage” used in PSE992+1217

WARNING
UNINTENDED EQUIPMENT OPERATION
Follow the recommendations for the maintenance given in the different chapters of this document, for each part of the device which is maintainable.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

VL “RiskEquipmentDamage_ThermalRunaway” used in PSE992

WARNING
HAZARD OF HEAT GENERATION
Power connections must never use other material than copper or aluminum.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

VL “Date_Not_Synchronized” used in PSE992

VL “maintenance_solvent” used in PSE1287

VL “maintenance_grease_Mobilith” used in PSE1287

VL “maintenance_grease_Mobilith” used in PSE1287

VL “LossDoubleIsolation” used in PSE1416 (translation existing in NVE40478)

VL “TerminalBlock_HoldSides” used in PSE1416 (repair procedures)

VL “information_updated” used in PSE992+1217+1287

The information contained in this document is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/docs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?