How to Maintain the Charging Mechanism

@TW: profiled topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Functions

The charging mechanism is used to close the main contacts.

Degradation Factors

The factors which can cause degradation of the charging mechanism are the following:

  • Dusty or dirty environment

  • Shocks

  • Corrosive atmosphere

  • Idle for long periods of time

Potential Hazards

Performing regular maintenance on the charging mechanism can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Charging mechanism is jammed.

Jammed mechanism

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the charging mechanism.

Maintenance program

Preventive action

Procedure

Routine end-user preventive maintenance

Operate the device manually and electrically.

Mechanism NII_Z_1

Mechanism NII_1_1

Mechanism NII_ZA_1

Charge the device electrically with MCH gear motor.

Mechanism NII_Z_2

Mechanism NII_1_2

Mechanism NII_ZA_2

Check the complete closing of the device poles.

Mechanism NII_Z_3

Mechanism NII_1_3

Mechanism NII_ZA_3

Intermediate end-user preventive maintenance

Check the MCH gear motor charging time at 0.85 Un.

Mechanism NIII_Z_1

Mechanism NIII_2_1

Mechanism NIII_ZA_1

Check the general condition of the mechanism.

Mechanism NIII_Z_2

Mechanism NIII_2_2

Mechanism NIII_ZA_2

Manufacturer preventive maintenance

Check opening and closing forces.

Contact your Schneider Electric Services representative.

Clean and regrease the mechanism.

For more information, refer to Preventive Maintenance Programs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?