Influence of Interrupted Currents on Aging

@TW: used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Interrupted Currents

Influence

Appearance

Consequences

Wear of fixed and moving contacts

Deterioration of contacts

Beyond the electrical-endurance limit, device temperature rise increases due to the greater contact resistance and a reduction in the pressure of contacts.

Wear of the arc chutes (insulating materials, separators)

Deterioration of insulation

Beyond the electrical-endurance limit, the insulation (input/output and between phases) is reduced, which results in a reduction of device suitability for isolation.

In this case, the safety of persons is not guaranteed.

Recommendations

The maintenance and installation recommendations according to the interrupted currents are defined in the following table:

Thresholds

Description

I/In ≤ 0.4

This level of interrupted current corresponds to the mechanical durability (see Mechanical endurance).

I/In ≤ 0.8

This level of interrupted current corresponds to approximately 125 % of the electrical durability.

I/In

This level of interrupted current corresponds to the electrical durability at the specified voltage (see Electrical endurance).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?