Influence of Temperature on Aging

@TW: used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Ambient Temperature Outside the Switchboard

The ambient temperature around the switchboard affects the device temperature, which is itself affected by the percent load.

Major variations in temperature (greater than 30 °C (86 °F)) cause both mechanical stresses (thermal expansion) and condensation, both of which can accelerate aging.

Influence

Appearance

Consequences

Aging of plastic insulation. Deterioration of the mechanical characteristics of plastic parts (insulation, case) for which deterioration speed is increased with temperature rise.

Change in color

Breaking of parts leading to potential failure of functions

  • Hardening of grease.

  • Elimination of grease on disconnecting contact clusters.

  • Change in color and viscosity

  • Caramel color of clusters

  • Device cannot be operated

  • Increase of racking forces exerted on clusters

Deterioration of insulating varnishes on coils.

Burning smell

Potential failure of coils (current transformers, MN, MX, or XF voltage releases, MCH gear motor, RES electrical remote reset)

Hardening of glues.

Visual

Loss of labels

Deterioration of electronic components.

Modified display of LCDs

  • Interruption of display

  • Nuisance tripping or no tripping

Deterioration of opto-electronic devices and SCRs.

Not identifiable

Possible transmission of erroneous orders

Interruption of battery backup power.

Not identifiable

Trip-cause indication not displayed

Recommendations

The maintenance and installation recommendations according to the annual average ambient temperature Ta are defined in the following table:

Annual average ambient temperature Ta

Description

Maintenance recommendations

Installation recommendations

< 25 °C (77 °F)

Optimum operating conditions

Implement the Intermediate program.

No particular recommendation

25 to 35 °C (77 to 95 °F)

A 10 °C (50 °F) increase in the ambient temperature is equivalent to a 5 % increase in the percent load.

Carry out more frequent periodic checks.

No particular recommendation

35 to 45 °C (95 to 113 °F)

A 20 °C (68 °F) increase in the ambient temperature is equivalent to a 10 % increase in the percent load.

Carry out more frequent periodic checks.

Install forced-air ventilation in the switchboard, or air conditioning for the electrical room.

Example: Influence of the ambient temperature on the service life for a 1,000 A device, with an 80 % load.

Annual average ambient temperature Ta

Typical service life of the device (electronic components excluded)

25 °C (77 °F)

30 years

35 °C (95 °F)

27 years

45 °C (113 °F)

25 years

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?