Library File novA Products
Micrologic X (PSE1061)
For information about recommended action on events, refer to the relevant document:
-
MasterPacT MTZ1 - Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Units - User Guide
-
MasterPacT MTZ2/MTZ3 - Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Units - User Guide
VL “X_EarthLeakageProtectionLoss” used in PSE1061(Micrologic X).
VL “24Vdc_SELV_use” used in PSE1061(Micrologic X).
VL “24Vdc_SELV_connection” used in PSE786 (ULP), PSE1061 (Micrologic X) incl. customized consequence (‘will result in a basic/single insulated system’).
Maintenance Procedures (PSE1217+1287+1416) and Maintenance Guide (PSE992)
VL “MaintenanceReco” used in PSE992+1217+1287+1416
VL “MaintenanceReco” used in PSE992+1217+1287+1416+ Compact NSX Twin PSE1539
Maintenance recommendations for each device are intended to maintain the equipment or subassemblies in a satisfactory operational state for their useful service life.
VL “MaintenanceOp” used in PSE992+1217+1287+1416+ Compact NSX Twin PSE1539
The following table summarizes maintenance operations for the three preventive maintenance programs:
Maintenance program |
Maintenance description |
Performed by |
---|---|---|
Routine end-user maintenance |
Visual inspection and functional testing, replacement of inoperative accessories. |
|
Intermediate end-user maintenance |
Routine end-user maintenance, plus operational servicing and subassembly tests. |
|
Manufacturer maintenance |
Intermediate end-user maintenance, plus diagnostics and part replacements by Schneider Electric Services. |
Schneider Electric Services representatives |
VL “MTZ_VPS” used in PSE1079 MTZ2/3
VL “MTZ_VPS” used in PSE1287 maintenance
VL "MTZ_safety_FixedCB" used in D-SE-0057794 (Breaking Unit NIII_Z_1: Check the Condition of the Breaking Unit)
VL "MTZ_safety_FixedCB" used in D-SE-0057803 (Chassis NIII_Z_1: Dust and Grease Chassis)
VL “GeneralSafety_RiskEquipmentDamage” used in PSE992+1217
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
Follow the recommendations for the maintenance given in
the different chapters of this document, for each part of the device
which is maintainable.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
VL “RiskEquipmentDamage_ThermalRunaway” used in PSE992
![]() |
---|
HAZARD OF HEAT GENERATION
Power connections must never use other material than copper
or aluminum.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
VL “Date_Not_Synchronized” used in PSE992
VL “maintenance_solvent” used in PSE1287
VL “maintenance_grease_Mobilith” used in PSE1287
VL “maintenance_grease_Mobilith” used in PSE1287
VL “LossDoubleIsolation” used in PSE1416 (translation existing in NVE40478)
VL “TerminalBlock_HoldSides” used in PSE1416 (repair procedures)
VL “information_updated” used in PSE992+1217+1287
The information contained in this document is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/docs.
VL “X_protective_cover” used in PSE1416 (repair procedures)