DUG_Wiser Micro Module Dimmer_CLP-00

About the device

The Wiser Micro Module Dimmer (hereinafter referred to as module) combines the advantages of smart dimmer functionality with ordinary mechanical push-button switches. It transforms a conventional switch into a connected device which can be controlled from the switch or through the Wiser app. It can switch and dim the ohmic, inductive, or capacitive loads and it is also compatible with dimmable LEDs.
NOTE: Do not control any devices that depend on a permanent power supply.

Additional features:

  • Remote control with maximum of 10 single mechanical push-buttons.

  • Setting the LED operating mode manually (RL LED mode).

  • Electronic overload protection, overheating protection, and short-circuit protection.

  • Setting the dimming range: minimum and maximum brightness.

  • Setting a time schedule.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?