DUG_IPC_Indoor_PDL–02

Inserting a micro-SD card

The micro-SD card is inserted in the device to store the recording.
NOTE: The micro-SD card has to be inserted before you power On the device. If the device is already in On state, then switch Off the device to insert the micro-SD card.

Follow the steps to insert a micro-SD card:

  1. Move the camera up to see the micro-SD card slot.
    TIP: If the IP camera is already in use, then use ˄ icon on the control panel to move the camera up.
  2. Insert a micro-SD card in the slot.
  3. Move the camera back to its initial position.
    Once the micro-SD card is inserted, you can configure the playback settings.
    NOTE: A maximum of 128 GB SDHC and SDXC micro-SD cards with FAT32 format are supported.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?