DM page

To view DM parameters:

  1. From the Home page, use Up or Down button to navigate to DM.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next DM parameter.
  4. Press Left button to exit.
Name on display Description
d.W Displays the last demand value for active power.
d.VA Displays the last demand value for apparent power.
d.VAR Displays the last demand value for reactive power.
Rd Displays the raising demand value.
tR Displays the time remaining, for example mm:ss.
NOTE: Maximum demand occurrence are displayed with 2 digit Minutes and 2 digit Seconds.
md Displays the maximum demand value.
md.oc Displays the Maximum demand occurrence time, for example hhhhhh:mm.
NOTE: Maximum demand occurrence are displayed with 6 digit Hours and 2 digit Minutes.
NOTE: Based on the selected power type under Demand setup, the DM page displays either DM W, DM VA, or DM VAR.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?