Meter overview

The PM1130H / EM6438H series meters are dual source meters that offer comprehensive 3-phase electrical instrumentation and load management facilities in a compact and rugged package.

The PM1130H / EM6438H meters offer value for the demanding needs of your energy monitoring and cost management applications. Meters in the series range comply with Class 0.5 (PM1130H & EM6438H) and Class 1.0(EM6438H) accuracy standards and feature high quality, reliability and affordability in a compact and easy to install format.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?