Network management

Your device can be used in various network management applications.

Some of the applications are as mentioned below:

  • Power quality analysis (THD %)

  • Demand measurement

  • Measurement of power factor

  • Phase angle between the voltage and current

  • % unbalance among voltage and current

  • Modbus RTU protocol RS-485 port for integration with energy management system

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?