Power quality (PM1130H) Power quality Power quality(EM1250H / EM1220H)

The meter provides complete harmonic distortion metering, recording, and real-time reporting, up to 15th harmonic for all voltage and current inputs (depending on the selected wiring configuration).

The following power quality measurements are available in the meter:

  • Total harmonic distortion (THD%) for current and voltage (displays line-to-line or line-to-neutral, based on selected wiring configuration)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?