Button functions in viewing setup parameters

Mode Button Description Function
Setup menu Down key: To navigate down To navigate to the next parameter configuration screen.
Up key: To navigate up To navigate to the previous parameter configuration screen.
Right / OK key: To navigate right / Enter key Enter setup mode to configure the displayed parameter value.
Mode Button Description Function

Setup menu

Left key: .To navigate left / Escape To navigate to the left or exit screen.
Down key: To navigate down To navigate to the next parameter configuration screen
Up key: To navigate up To navigate to the previous parameter configuration screen.
Right / OK.key: To navigate right / Enter key Enter setup mode to configure the displayed parameter value.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?