Clear screen menus

Clear screen enables you to reset energy, demand, or max demand values.

The meter allows you to clear the values only through communication.

Clear parameters

Parameters Description
MD

Resets the maximum demand values under Demand.

  • W, VA, and VAR with timestamp

Enrg

Resets the Energy values and Run Hours under INTG.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?