Setup parameters

Name on display Description Input range Default value

TYPE

TYPE: Power System Configurations [1P.Ln, 1P.LL, 1P.3L, 3P.3L, 3P.4L]
NOTE: Other power system configurations can be set through ION setup.
3P.4L

VT

VT: Voltage Transformer [no.Vt, 2.VT, 3.VT, 1.VT]
NOTE: The VT Connect parameters are enabled based on selected power system configuration.
no.Vt

VT.PR

Vt.Pr: Primary Voltage (V L-L) [0100 V to 999000 V]
NOTE: VT.PR will not be enabled if VT Connect is no.VT.
415

VT.SE

Vt.SE: Secondary Voltage (V L-L) [100, 110, 115, 120, 415]
NOTE: VT.SE will not be enabled if VT Connect is no.VT.
415

CT

Ct: Current Transformer [A.1, A.2, A.3, A.12, A.23, A.31, A.123]
NOTE: The CT terminal parameters are enabled based on the selected power system and VT connect configuration.
A.123

CT.PR

Ct.Pr: CT Primary [1 A to 32760 A]
NOTE: CT primary can be set to 32767 A through communication.
100

CT.SE

Ct.SE: CT Secondary [1 A, 5 A] 5

FREQ

FrEq: System Frequency [50 Hz, 60 Hz] 50

A.SUP

A.SUP: A.Suppression (Minimum current at which meter starts functioning) [5 to 99 mA] 005

LABL

LABL: Phase labeling [123, Abc, rst, pqr, ryb] 123

FS%

FS%: Full scale value (Rescaling analog load bar with respect to CT loading) [1 to 100] 100

P.SEL

P.SEL: Parameter selection [VA, W, VAR] W

POLE

POLE: To determine RPM of alternator / generator based on number of poles and network frequency [2, 4, 6, 8, 10, 12, 14, 16] 4

SRC 1

SRC1: Source 1 [0 to 9, a to w, y] U

SRC 2

SRC2: Source 2 [0 to 9, a to w, y] G

PD

PD: Power demand [t.sb, t.b, t.rb] t.b

PD.CY

PD.CY: Demand period [1-60 min] 15

PD.UT

PD.UT: Demand update time [1-60 min] 15

PD.P

PD.P: Demand parameter [VA, W,VAR] VA

LED

LED: LED parameter [OFF, INTG] OFF

L.PLS

L.PLS: Pulses per energy [1 to 9999000] 1

COMM

COMM: Communication
  • ON / OFF: To enable / disable communications port.

  • Retrofit (RTFT): For configuring legacy communication data models.

[ON, RTFT, OFF] ON

ID

ID: Unit ID [1-247] 1

BAUD

BAUD: BPS (Baud rate per second) [4800, 9600, 19200, 38400] 19200

PRTY

PRTY: Parity [Even, Odd, None] Even

PASS

PASS: Password Can be configured from 0000 to 9999
NOTE: Record your password in a secure location.
0000
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?