Display screen menu tree
PM1130H parameter navigation
The below image summarizes the RMS parameters under PM1130H meter:

Favourite page (PM1130H)
The meter allows you to select 3 parameters and arrange them in required order to be displayed in favourite page. These parameters can be selected only through communication and are based customer requirements. Some parameter logs are of utmost importance and navigating to those parameters takes time. For ease of navigation and accessibility, the meter allows you to chose 3 parameters and lock the page for easy reading. The selectable parameters are:
-
V L-L
-
V L-N
-
A
-
F
-
W
-
PF
EM6438H parameter navigation
The below image summarizes the RMS parameters under EM6438H meter: