Smart keys

Operating the meter is easy, using the four smart keys to navigate through the display pages. The display pages expand as you go to the right, much like the directory or explorer tree displayed on any computer. The display shows where you are headed. The meter has four smart keys to navigate through the display pages. The display shows where you are headed.

Smart keys description

Right key / OK key
  • Going forward into sub-parameter pages.

  • To enter into Setup page. This action requires password.

  • Selecting the parameter to edit under Setup.

Left key
  • Going back to the main parameter pages.

  • Selecting previous digit on the left, under setup.

  • Exiting from editing Setup page.

Up key
  • Scrolling up through display pages at the same level, within the same function.

  • Increasing the value of the selected digit or navigating to the next available selection.

Down key
  • Scrolling down through other display pages at the same level, through all functions.

  • Decreasing the value of the selected digit or navigating to the next available selection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?