Keypad operation EM6438H

Press a key in the direction you want to go. The display shows the next parameter as per navigation. Press OK to enter a parameter setup.

The following steps explain how to navigate from the RMS page to the RPM page.

  1. From the RMS page, press right button. The display shows W PF.

  2. From W PF, press right button. The display shows W 123.

  3. Press down button, the display shows PF 123.

  4. Press down button, the display shows RPM.

NOTE: Use right button to go forward to the sub-parameter page and use left button to go backward to the main parameter pages. Use up button and down button to scroll up and down through the display pages.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?