Password setup
- From the Home page, use Up or Down button to navigate to Maintain.
- Press OK.
- Use Up or Down button to navigate to Set.
- Press OK.
- Enter password. Default password is 0000.
- Press OK.
- Press the Up button to select PASS (password) parameter.
- Press OK.
-
Press the Down or Up button to change the digits.
NOTE: Use the Left button to move the cursor to the next digit.
- Press OK.
- Press Left button.
- Select Yes (press OK button) to save your settings.
Password settings
Parameter | Values | Description |
---|---|---|
Pass | 0000 - 9999 | Sets the password for accessing the meter setup screen.
NOTE: Common password applies across all parameters.
|
Lost password
Visit www.se.com www.usa.siemens.com/pds for support and assistance with lost passwords or other technical problems with the meter. Make sure you include your meter’s model, serial number, and firmware version in your email or have it readily available if calling Technical Support.