Diag page

To view Diag parameter:

  1. From the Home page, use Up or Down button to navigate to Diag.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next Diag parameter.
  4. Press Left button to exit.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?