I/O page (PM1130H only)

To view I/O parameter:

  1. From the Home page, use Up or Down button to navigate to I/O.
  2. Press OK.
  3. Press Left button to exit.
Name on display Description
RLY Displays the relay – ON / OFF (Default)
BAL.U Displays the prepaid energy balance – Utility
BAL.G Displays the prepaid energy balance – Alternate source
BAL.T Displays the prepaid energy balance – Total (Utility + Alternate source)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?