Viewing parameters

The meter’s display screen and buttons allow you to view the required parameters.
To view display parameters:
  1. Press the Up or Down button to navigate to RMS menu.
  2. Press OK.
  3. Press the Up or Down button to navigate to the previous or next parameter page.
  4. Press the Left button to exit the navigation
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?