Displaying harmonics data

The meter displays voltage and current THD%. Phase wise THD% data can be read through communication also. The meter displays voltage and current THD%, refer to THD% page .
  1. From the Home page, use Up or Down button to navigate to THD.
  2. Press OK.
  3. Use Up or Down button to navigate to next THD screen.
  4. Press Left button to exit.
NOTE:

The LED rows display V1THD%, V2THD%, and V3THD% for VTHD% values, and V12THD%, V23THD%, V31THD%, and A1THD%, A2THD%, and A3THD% for ITHD% values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?