Tot INTG

Applicable for METSEPM1125HCL1LVD / METSEPM1125HCL5LDD

Applicable for METSEPM1130HCL5LVD

Applicable for METSEEM6433HCL5LVD / METSEEM6436HCL5LVD / METSEEM6459HCL5LVD

To view tot INTG parameters:

  1. From the Home page, use Up or Down button to navigate to Tot INTG.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next Tot INTG parameter.
  4. Press Left button to exit.

Name on display

Description

Wh. u

Displays the active energy for utility

Rh. u

Displays the run hours for utility, for example: hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

Wh. G

Displays the active energy for generator

Rh. G

Displays the run hours for generator, for example: hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

Wh. t

Display the Active energy for total

Rh. t

Display the Run hours for total, for example: hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

Name on display

Description

d. wh

Displays the delivered active energy

d. VRh

Displays the delivered reactive energy

d. VAh

Displays the delivered apparent energy

d. Rh

Displays the delivered run hours, for example hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

R. wh

Displays the received active energy

R. VRh

Display the received reactive energy

R. VAh

Displays the received apparent energy

R. Rh

Displays the received run hours, for example hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

t. wh

Display the total active energy

t. VRh

Displays the total reactive energy

t. VAh

Displays the total apparent energy

t. Rh

Displays the total run hours, for example hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

Name on the display

Description

Wh.

Displays the active energy

Rh

Displays the run hours, for example: hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?