Tot INTG
Applicable for METSEPM1125HCL1LVD / METSEPM1125HCL5LDD
Applicable for METSEPM1130HCL5LVD
Applicable for METSEEM6433HCL5LVD / METSEEM6436HCL5LVD / METSEEM6459HCL5LVD
To view tot INTG parameters:
- From the Home page, use Up or Down button to navigate to Tot INTG.
- Press OK.
- Press the Up or Down button to navigate to the next Tot INTG parameter.
- Press Left button to exit.
Name on display |
Description |
---|---|
Wh. u |
Displays the active energy for utility |
Rh. u |
Displays the run hours for utility, for example: hhhhhh:mm NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.
|
Wh. G |
Displays the active energy for generator |
Rh. G |
Displays the run hours for generator, for example: hhhhhh:mm NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.
|
Wh. t |
Display the Active energy for total |
Rh. t |
Display the Run hours for total, for example: hhhhhh:mm NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.
|
Name on display |
Description |
---|---|
d. wh |
Displays the delivered active energy |
d. VRh |
Displays the delivered reactive energy |
d. VAh |
Displays the delivered apparent energy |
d. Rh |
Displays the delivered run hours, for example hhhhhh:mm NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.
|
R. wh |
Displays the received active energy |
R. VRh |
Display the received reactive energy |
R. VAh |
Displays the received apparent energy |
R. Rh |
Displays the received run hours, for example hhhhhh:mm NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.
|
t. wh |
Display the total active energy |
t. VRh |
Displays the total reactive energy |
t. VAh |
Displays the total apparent energy |
t. Rh |
Displays the total run hours, for example hhhhhh:mm NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.
|
Name on the display |
Description |
---|---|
Wh. |
Displays the active energy |
Rh |
Displays the run hours, for example: hhhhhh:mm NOTE: Run Hours are
displayed with 6 digit Hours and 2 digit Minutes.
|