Meter configuration using ION setup

Start ION setup, create a site (or if applicable, use an existing site), then add your meter to the site.

See the “EasyLogic PM2000 Series Power Meter” topic in the ION setup online help or in the ION setup device configuration guide. To download a copy, go to www.se.com www.usa.siemens.com/pds and search for ION setup device configuration guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?