Accuracy test requirements
Signal and power source
The meter maintains its accuracy during voltage and current signal source variations but its energy pulsing output needs a stable test signal to help produce accurate test pulses. The meter’s energy pulsing mechanism needs approximately 10 seconds to stabilize after every source adjustment.
The meter must be connected to control power in order to conduct accuracy verification testing. Refer to your meter’s installation documentation for power supply specifications.
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION,
OR ARC FLASH
Verify the device’s power source
meets the specifications for your device’s power supply.
Failure to follow these instructions will result in death or serious injury.
|
Control equipment
Control equipment is required for counting and timing the pulse outputs from an energy pulsing LED.
-
Most standard test benches have an arm equipped with optical sensors to detect LED pulses (the photodiode circuitry converts detected light into a voltage signal).
-
The reference device or energy standard typically has digital inputs that can detect and count pulses coming from an external source (i.e., the meter’s pulse output).
Environment
The meter should be tested at the same temperature as the testing equipment. The ideal temperature is about 23 ºC (73 ºF). Make sure the meter is warmed up sufficiently before testing.
A warm-up time of 30 minutes is recommended before beginning energy accuracy verification testing. At the factory, the meters are warmed up to their typical operating temperature before calibration to help ensure that the meters will reach their optimal accuracy at operating temperature.
Most high precision electronic equipment requires a warm up time before it reaches its specified performance levels. Energy meter standards allow the manufacturers to specify meter accuracy derating due to ambient temperature changes and self-heating.
Your meter complies with and meets the requirements of these energy metering standards.
For a list of accuracy standards that your meter complies to, contact your local Schneider ElectricSiemens Industry representative or download the meter brochure from www.se.comwww.usa.siemens.com/pds.
Reference device or energy standard
To help ensure the accuracy of the test, it is recommended that you use a reference device or reference energy standard with a specified accuracy that is 6 to 10 times more accurate than the meter under test. Before you start testing, the reference device or energy standard should be warmed up as recommended by its manufacturer.