I/O ModulesInput / Output

NOTE: Applicable only for PM2230 meter model Applicable only for PM2230R meter modelApplicable only for PM2130 meter model

This section supplements the optional I/O module installation sheets and provides additional information regarding physical characteristics and capabilities of the I/O module.

The I/O modules are available in the following variants:

  • Single channel analog I/O module

  • Two channel analog I/O module

  • Two channel digital I/O module

  • Two channel digital input and relay output module

This section supplements the input and output installation and provides additional information regarding physical characteristics and capabilities

The input and output are available in the following variants:

  • PM2125CPM2225CPM2225CR two channel analog input and output

  • PM2125CPM2225C two channel digital input and output

  • PM2125CPM2225CPM2225CR two channel digital input and relay output

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?