Setting up alarms using ION Setup

You can use ION Setup to create and set up alarms.
  1. Start ION Setup and connect to your meter.
  2. Open the Alarming screen.
  3. Select the alarm you want to configure and click Edit.
  4. Configure the setup parameters as explained in the different alarm setup sections.

    See the ION Setup Device Configuration guide for more information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?