Setting up the display

You can change the display screen’s settings, such as contrast, backlight timeout, and screen timeout .
  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to HMI > Disp.
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press the up arrow to exit.
  8. Press Yes to save your changes.

    Display settings available using the display

    Parameter

    Values

    Description

    Contrast 1 - 9 Increase or decrease the value to increase or decrease the display contrast.
    Backlight Timeout (min) 0 - 60 Set how long backlight reduces its brightness after inactivity minutes. Default setting “0” disables the backlight timeout feature (i.e., backlight is always ON).
    Screen Timeout (min) 0 - 60 Set how long the screen turns off after inactivity minutes. Default setting “0” disables the screen timeout feature (i.e., display is always ON).

    To configure the display using ION Setup, see the “PM2000” topic in the ION Setup online help or in the ION Setup device configuration guide, available for download at www.se.comwww.usa.siemens.com/pds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?