Configuring the preset energy using ION Setup

NOTE: Not applicable for MID/MIR meter models.

You can use ION Setup to configure the preset energy values.

  1. Start ION Setup .
  2. Connect to your meter.
  3. Open the Preset Energy screen.
  4. Click Edit to configure the Setup parameters as required.
  5. From the list, set the Preset Energy value for each parameter.
  6. Click Send to save your changes to the meter.

    Preset Energy parameters available using the ION Setup

    Parameter

    Values

    Description

    Active Energy Delivered

    Active Energy Received

    Reactive Energy Delivered

    Reactive Energy Received

    Apparent Energy Delivered

    Apparent Energy Received

    0 to 9.2233 E

    Use this field to enter the preset energy values

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?