7EN72-0203-02

Before you begin

Download latest ION Setup

To upgrade your meter to firmware version 2.1.0, you must use ION Setup version 3.1 or later.

  1. Start ION Setup.

  2. Click Help > About ION Setup to determine your ION Setup version.

  3. Open a web browser and go to https://www.se.com/en/download/document/ION_Setup_Latest_Release/ to locate the latest version of ION Setup.

  4. If you do not have the most recent released version, download the installation file, then run it to upgrade ION Setup.

Ensure you back up all your meter data and any custom templates, frameworks or files before proceeding with the upgrade.

Back up custom meter webpages

If you added new meter webpages or if you have customized the meter’s existing webpages, back up the webpage files.

NOTICE
loss of custom webpages
Back up your custom webpages before upgrading the meter firmware. The webpages upgrade process overwrites all existing meter webpages.
Failure to follow these instructions can result in loss of custom webpage functionality.

To back up your meter webpages, use an FTP client to log in to your meter, then copy the web folder to a local folder on your computer.

Back up custom meter frameworks

If your meter uses a custom meter template or if you have customized any of your meter frameworks, it is recommended that you back up your meter template in case you need to recreate or relink ION modules.

NOTICE
loss of custom frameworks
Back up your custom frameworks before upgrading the meter firmware. The upgrade process overwrites existing meter frameworks.
Failure to follow these instructions can result in loss of custom framework functionality.

To back up your meter template

  1. Start ION Setup and connect to your meter.

  2. Navigate to Setup Assistant > Template > Save to PC.

  3. Click Save.

  4. Navigate to the desired location and click Save.

QR code for this page

Was this helpful?